CMP#.WIDTHTYPE
Description
CMP#.WIDTHTYPE sets the type of duration of the output pulse generated by the setpoint Setpoint is the target value that an automatic control system, for example PID controller, will aim to reach. The duration can be either a value in the same units as CMP#.VAL or a time in ms.
It takes two command line arguments: the first specifies the setpoint, and the second specifies the duration type.
Examples
Usage
0: Value in CMP#.SOURCE units (default)
1: Time in ms
Code
The following commands set the duration for channel 1 setpoint 2 to value type, and channel 2 setpoint 7 to time type
--> CMP1.WIDTHTYPE 2 0
--> CMP2.WIDTHTYPE 7 1
Context
For more information please refer to Compare.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-06-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.